TGML Upgrade Utility

Use this tool to update restored TGML files. It is only required when upgrading to Power Operation 2024 R1.

  1. Open the Power Operation folder.

  2. Open the TGML Upgrade Utility program.

  3. Enter a location for Path to .tgml and .tgmlcomponent files. This is the location of TGML files and components.

  4. Click Upgrade.